The ’AHC86 devices are quadruple 2-input exclusive-OR gates. These devices perform the
Boolean function Y = A ⊕ B or Y = AB + AB in positive
logic.
A common application is as a true/complement element. If one of the inputs is low, the
other input is reproduced in true form at the output. If one of the inputs is high, the signal on
the other input is reproduced inverted at the output.
View datasheet View product folder