See datasheet for actual packaging/pinout drawings


TUSB2136-TPS2149 Product Development Kit

TI Store Price:

Unit price: $149.00

Adjust your quantity during checkout

Texas Instruments TUSB2136TPS2149PDK

The TUSB2136TPS2149PDK can be used to evaluate the TUSB2136 USB compound hub device and the TPS2149 USB power controller device in a keyboard application. Both a main evaluation module and a mini keyboard are included in the TUSB2136TPS2149PDK. The user is expected to be familiar with 8052 MCU architecture and programming, as well as USB certification requirements. For more information on Universal Serial Bus and certification, logo, and testing requirements, see

Software/Utilities Available include:

  • AppLoader is a Windows-based USB Device Driver that will load binary 8052 code to the TUSB2136. It allows the user to keep the firmware on the PC rather than in an EEPROM on the board. The EEPROM must be removed from the board for Apploader to function. When the device is plugged into the PC, Windows associates it with this driver, which then downloads the firmware to the device's RAM directly. AppLoader has been tested under Win98SE, Win2K, WinME and WinXP. It is intended to be used during the firmware development phase of a project and is not intended for production use. Firmware on production systems should be stored on an EEPROM in the USB device.
  • The I2C Header Generator Utility is a DOS-based tool that generates an image file for your I2C EEPROM, using your binary object code and/or custom descriptors as inputs.
  • The Sample Source Code can be downloaded if you agree to the online royalty-free license agreement. Objext code comes pre-loaded in the on-board EEPROM. If you will do your own firmware devlopment, a Compiler will be required. Since the TUSB2136 is based upon the industry-standard 8052 microcontroller, there are several compilers on the market that would be suitable. Some examples are at,, and at

The TUSB2136/3210 Firmware Debugging Guide is a general instruction guide on how to debug user-developed firmware using the TUSB2136's native 8052 debug port.

The TUSB2136/3210/5052 USB Firmware Architecture 8052 Embedded USB Micro-Controller document discusses the firmware architecture of the TUSB3210.

Additional items needed for EVM use include a USB Montioring Utility and a USB enabled Host computer.

Order SummaryEdit >
Subtotal: $0.00
Shipping & Handling: -
Total (USD): $0.00